LibJpeg.NET, LibTiff.Net

The Bit Miracle's JPEG software
===============================
Please send bug reports, offers of help, etc. to support@bitmiracle.com

This package contains C# software to implement JPEG image compression and
decompression.  JPEG (pronounced "jay-peg") is a standardized compression
method for full-color and gray-scale images.  JPEG is intended for compressing
"real-world" scenes; line drawings, cartoons and other non-realistic images
are not its strong suit.  JPEG is lossy, meaning that the output image is not
exactly identical to the input image.  Hence you must not use JPEG if you
have to have identical output bits.  However, on typical photographic images,
very good compression levels can be obtained with no visible change, and
remarkably high compression levels are possible if you can tolerate a
low-quality image.  For more details, see the references, or just experiment
with various compression settings.

This software implements JPEG baseline, extended-sequential, and progressive
compression processes.  Provision is made for supporting all variants of these
processes, although some uncommon parameter settings aren't implemented yet.
For legal reasons, we are not distributing code for the arithmetic-coding
variants of JPEG; see LEGAL ISSUES.  We have made no provision for supporting
the hierarchical or lossless processes defined in the standard.

We provide a set of library routines for reading and writing JPEG image files,
plus two sample applications "cjpeg" and "djpeg", which use the library to
perform conversion between JPEG and some other popular image file formats.
The library is intended to be reused in other applications.

In order to support file conversion and viewing software, we have included
considerable functionality beyond the bare JPEG coding/decoding capability;
for example, the color quantization modules are not strictly part of JPEG
decoding, but they are essential for output to colormapped file formats or
colormapped displays.  These extra functions can be compiled out of the
library if not required for a particular application.

We welcome the use of this software as a component of commercial products.
No royalty is required, but we do ask for an acknowledgement in product
documentation, as described under License.

License
=======
Please read License.txt

This software is copyright (C) 2008-2011, Bit Miracle
http://www.bitmiracle.com

This software is based in part on the work of the Independent JPEG Group
Copyright (C) 1991-1998, Thomas G. Lane.
All Rights Reserved except as specified below.

LEGAL ISSUES
============

It appears that the arithmetic coding option of the JPEG spec is covered by
patents owned by IBM, AT&T, and Mitsubishi.  Hence arithmetic coding cannot
legally be used without obtaining one or more licenses.  For this reason,
support for arithmetic coding has been removed from the free JPEG software.
(Since arithmetic coding provides only a marginal gain over the unpatented
Huffman mode, it is unlikely that very many implementations will support it.)
So far as we are aware, there are no patent restrictions on the remaining
code.