16. Jan. 2023 File is password protected, upon customer request to services.didactic@festo.com "7-Zip File Image for Machine Learning on Raspberry Pi" 1) Download the 7-Zip file "ML_RPi.7z.zip" (>6 Giga Byte) rename it to "ML_RPi.7z" 2) Unzip it with 7-Zip 3) An image file of about 16 GB should be build 4) To flash the image on a SD card please follow the provided PDF tutorial 5) Once the SD card has been flashed put the card back into the Raspberry Pi and power it on 6) Wait for 2-3 minutes (during the very first boot of a new image, some rearrangements wrt. the memory system will be executed) 7) Go to the MES4 PC (first MPS Station) 8) Open Google Chrome and enter "172.21.55.46:5000" to open the machine learning web interface 9) For more information on how to use the ML-based image classification visit the FestoLX course "Artificial Intelligence in Production"