Update procedure: -------------------------------------------------------------------------------------------------------------------- 1. Rename the existing folder "FactoryViews" on the MES PC (under C: or C:\FestoDidactic), e.g. to FactoryViews_old. 2. Download and execute FactoryViews.exe and move the created folder "FactoryViews" to the original location 3. Execute the file "Setup.bat" and press "1"-key "1) Refresh now!" to start the routine 4. Download and unzip "htdocs.zip" (includes InfoPortal offline, >15 GB) to the new directory "FactoryViews\XAMPP\htdocs" 5. Start "FactoryViews - ControlPanel.exe" 6. Create and replace a shortcut to "FactoryViews - ControlPanel.exe" on the desktop