These are the target support packages (TSP) for the CoDeSys programming environment to program the soft PLC of the camera. TSPs 3.0.x are for camera firmware 3.40. TSPs 3.5.x are for camera firmware 3.50. The parallel installation of TSPs 3.0.x and 3.5.x is possible. A detailed installation instruction is inside the CAA-Merger-1.chm. (i.e. Help\English\CAA-Merger-1.chm of the unpacked archive) at chapter [Preliminary work][Preparing the PC] at section "Installation of the target system" The firmware version of your camera can be checked acc. to chapter [Preliminary work][Preparing the SBO..-Q Compact Vision System] at section "Checking the firmware version" First startup examples can be found at directory "Examples" of the package. These are also installed to the development PC during TSP installation. (i.e. c:\Program Files\Festo\CoDeSys V2.3\Targets\Festo or c:\Program Files (x86)\Festo\CoDeSys V2.3\Targets\Festo) All TSP changes are available via the IOCONFIG\Changelog.txt (of the unpacked archive). This changelog is also installed to the development PC during TSP installation. Release History: ================ SBOx-Q Firmware 3.50 -------------------- 2011-Sep-22 (build 1205): SBOx-Q_3_5_4.zip SBOx-Q Firmware 3.40 -------------------- 2011-Oct-11 (build 1212): SBOx-Q_3_0_12.zip (bugfixed, backported 3.5.4) 2010-Jul-27 (build 946): SBOx-Q_3_0_8.zip 2010-Apr-23 (build 848): SBOx-Q_3_0_6.zip