_____ v 2.0.2.1 - bugfixing on show finished orders with error in the suborders - changed from XAMPP to a stand alone MairaDB _____ v 2.0.2.0 - add replaning do on op end _____ v 2.0.1.14 - updated MySQL v 2.0.1.13 - add Special SQL to reload resources states Messages 1/5 - add ip Adresses when load standard RSCs _____ v 2.0.1.12 - solved bug if Robotino drives from CP-Lab to CP-Lab _____ v 2.0.1.11 - added HTML Page and PLC Type to import function - changed color of comments - add new colored Text in SQl-Editor - Error occures after 30s no DB Connection _____ v 2.0.1.10 - new cryption _____ v 2.0.1.9 - bugfixing - sign _____ v 2.0.1.8 - correct bug for different resources with same IP-Address _____ v 2.0.1.7 - changed wayfinding for Robotino - Bugfixing Maintenenace Orders - Bugfixing finish Maintenenace Orders _____ v 2.0.1.6 - bugfixing _____ v 2.0.1.5 - fixed bugs on cyclic task handling like OpNo 1040 _____ v 2.0.1.4 - bugfixing _____ v 2.0.1.3 - bug solved that slowed down the String communication _____ v 2.0.1.2 - other error handling on startup if the database is not started yet _____ v 2.0.1.1 - send carrierID on OPStart now possible - send ONo OPos, ... back on OPStart _____ v 2.0.1.0 - change querry getOpForCarrier - reload after db changed Message 1/2 - Bugfixes _____ v 2.0.0.0 - switch to MySQL - added parameter claculate on dispatch - added parameter for active step or not - added port for MySQL connection string - added new Table to handle ONos in MySQL selection - Jump to defined Errorstep on Returncode XXX --> possible with do on OpEnd and #ErrorCode variable - Comments in OpEnd MySQL Command and Parameter on Runtime possible - start MES4 minimized and it is possible to open full UI --> To Do: activate this from config file - added lastLocation and DateTime to tblCarrier, to identify the last location to write thes every Querry in MClass 100 write it to the DB if RSC an Stopper pos and Carrier ID is send - add bit to control lite mode of MES4 (max 3 Resources) - show a correct Error Log - open error log without Main Visu - switch program to 64bit - background optional (config.xml) - solved error on creating customer - add special operation 1100 to call a sql statement and check return values - Add OPC UA Config variable to tblResource - Change DB from isam to inodb --> may be slower by big tables - correct automatic orders --> no error on opening now - add query to get MES4 and DB Version as string MClass/MNo 1/1 - add tblDBinfo to DB --> version of DB and short comment _____ v 1.2.2.3 - Bugfix on the PartGroups _____ v 1.2.2.2 - Bugfix on the menu for the BufferZones _____ v 1.2.2.1 - Bugfix after Windowsupdate (20H2 OS build 19042.1288) that slowed down the string communication over TCP _____ v 1.2.2.0 - SetRscForStepNo is now possible, we can plan a station dynamicaly that do that operation --> only CP-Lab, Only use in the step before _____ v 1.2.1.9 - change parameter to force - Bugfix on calculate resource _____ v 1.2.1.8 - Bugfix on delete Rsc - Bugfix on Book Order in Box _____ v 1.2.1.7 - new resource files for CP-Systems - Bugfix resource library - add delete option for resources on right click - Bugfix on import buffers for Box-Storage - set Robtino topologie to 10 possible dockings _____ v 1.2.1.6 - add copy to clipboard to PLC-Sim - add querry 101/6 to create a new customer order (PNo and changable parameters are sent in a string) - installation of ODBC for access if it is needed _____ v 1.2.1.5 - bug solved to show strings in changeable combo box _____ v 1.2.1.4 - bug solved in workplan creation first step _____ v 1.2.1.3 - bug solved in alternative step _____ v 1.2.1.2 - bug solved on edit parameter for operations - new standard DB corrections ASRS12 and MEAS operations. Add standard maintenance orders to db - bug solved in MaintOrders _____ v 1.2.1.1 - bug solved on add a new buffer _____ v 1.2.1.0 - implement stack magazine option for maintenance storage - new Querry 151/11 DelBufPos - Change SetBufPos 151/10 to book Quantity in stack buffer with Aux1Int - Change GetBufPos to get quantity in Aux1Int - longer textbox for part number in order entry _____ v 1.2.0.2 - bug solved on edit parameter in Operations _____ v 1.2.0.1 - DB changes: add Rows, Columns, Sides to tblBuffer - change ui to add Buffers - fixed bug: initial folder load DB - fixed bug: set new customers - add and change Lib for standard Rscs _____ v 1.1.5.1 - fixed bug: MES4 can handle now string parameter generation on Runtime - fixed bug: Show Picture of Workpiece on Details on Runtime - ping stations directly from MES4 from RSC Window _____ v 1.1.5.0 - Tooltip for Positions, to show variable parameters in customer orders - fixed bug in Workplan Window _____ v 1.1.4.1 Bugfix: calculate resources _____ v 1.1.4.0 Feature: - handle order with no Rsc - Handle more then one Rsc for the same Operation - set checkbox in WP-Creation to show all operations